I/O Configuration
This allows you to set the function, polarity, and Out data for each pin of the instrument.
| Function | Select the digital I/O function for the pin from the dropdown list. The options depend on the pin and the instrument. |
| Polarity | Configure the polarity for the pin (Positive or Negative). |
| In | This reflects the condition of the external signal that is applied to the pins. |
| Out | Selected - a binary bit 1 with positive polarity specifies a voltage high at the pin. Not selected - a binary bit 0 with positive polarity specifies a voltage low at the pin. |